AD8333
Production
The AD8333 is a dual-phase shifter and I/Q demodulator that enables coherent summing and phase alignment of multiple analog data channels. It is the first...
Datasheet
AD8333 on Analog.com

Hi,
The RSET pin is used to synchronize the LO dividers in AD8333 arrays.Please refer attached AD8333_Final_Approval.pdf
Synchronization of multiple AD8333s can be checked as follows:
1. Set the phase code of all AD8333 channels to the same
setting, for example, 0000.
2. Apply a test signal to a single channel that generates a sine
wave in the baseband output, and then measure the output.
3. Apply the same test signal to all channels simultaneously,
and then measure the output.
And also refer here https://ez.analog.com/amplifiers/f/q-a/15060/simulating-ad8333/126912#126912
Thanks,
Poornima
Hi,
The RSET pin is used to synchronize the LO dividers in AD8333 arrays.Please refer attached AD8333_Final_Approval.pdf
Synchronization of multiple AD8333s can be checked as follows:
1. Set the phase code of all AD8333 channels to the same
setting, for example, 0000.
2. Apply a test signal to a single channel that generates a sine
wave in the baseband output, and then measure the output.
3. Apply the same test signal to all channels simultaneously,
and then measure the output.
And also refer here https://ez.analog.com/amplifiers/f/q-a/15060/simulating-ad8333/126912#126912
Thanks,
Poornima
Thank you. I will do that by following your tips.