ADN4654 FPD-Link I usage

Hello,

Is it possible to isolate lvds signals used in FPD-Link I (1 differential clk and 5 differential data pairs) with ADN4654? Since duty cycle of clock signal is not %50, it will have DC component. Can ADN4654 handle this?

Thanks,

Gurkan

Parents
  • +1
    •  Analog Employees 
    on Mar 12, 2019 2:31 PM

    ADN4654 can be used to isolate FPD-Link I and other similar LVDS-based links like Camera Link/Channel Link.

    The isolator can be used for any arbitrary data rate, right down to a DC state. So there is the capability to isolate all sequences and states, including those that are not AC-balanced.

    As well, there's even a "refresh" mechanism that ensures any DC state at the output remains correct even if there are no further transitions. This is useful in any scenario that's outside the common-mode transient specification of 25 kV/us for example.

Reply
  • +1
    •  Analog Employees 
    on Mar 12, 2019 2:31 PM

    ADN4654 can be used to isolate FPD-Link I and other similar LVDS-based links like Camera Link/Channel Link.

    The isolator can be used for any arbitrary data rate, right down to a DC state. So there is the capability to isolate all sequences and states, including those that are not AC-balanced.

    As well, there's even a "refresh" mechanism that ensures any DC state at the output remains correct even if there are no further transitions. This is useful in any scenario that's outside the common-mode transient specification of 25 kV/us for example.

Children