Post Go back to editing

ADV7181C I2C access

Thread Summary

The user encountered issues reading data from the ADV7181C video serialiser via I2C. The solution involves writing to the index register address first, then sending a repeat start before reading the data. The manual confirms that the master must NACK the last byte to stop the read sequence, which is specific to this device. The user also found the design support files helpful for register configuration.
AI Generated Content

We are at the early stages of debugging a video board using the ADV7181C video serialiser.

When I write (R/W = W) a command through the I2C interface to the chip using address 0x21 (or 0x42 as stated in the manual) I receive an ack per each byte sent. This is good

But when I try to receive data (R/W = R) from this same address the address byte is not acknowledged and of course no communication takes place.

The manual creates some confusion in my mind about the I2C address, should it be shifted, should it not! Although I've tried all possible addresses and the only that is acknowledged when writing is in fact 0x21.

Could anyone give me some ideas about this?

thanks

  Eduardo

  • I was able to find some clue about the abnormal behaviour related before.

    According to the ADV7181C_Manual_RevC.pdf a read sequence should be as follows (see also the picture attached):

    START  SlaveAddr  Ack(Slave)  SubAddr  Ack(Slave)  START  SlaveAddr  Ack(Slave)  Data  Ack(Master)  ...  Data  /Ack(Master)  STOP

    Apparently the ADV7181C expects two START bits in order for a read sequence to be done.

    Can some one acknowledge that this is the proper way to do a read?

    thanks

  • FormerMember
    0 FormerMember
on Nov 20, 2012 2:15 PM

Reading back is a 2 step process. First you write the index register address you want to read back from and then send another Start bit, slave read address and then read back the data.  The second Start is sometimes referred to as a repeat start.

  • thanks for your answer.

    It is working now

    Allow me another question.

    In the same context the frame to be sent is:

    START  SlaveAddr  Ack(Slave)  SubAddr  Ack(Slave)  START  SlaveAddr  Ack(Slave)  Data  Ack(Master)  ...  Data  /Ack(Master)  STOP

    For some reason the manual indicates that the last byte of Data should be NOT Acknowledged by the Master.

    Is this the proper action? (I thought that the transfer of data from the slave would be terminated when the master used the STOP.)

  • In Read Mode, the highest subaddress register contents continue to be output until the

    master device issues a no-acknowledge. This indicates the end of a read. A no-acknowledge

    condition is where the SDA line is not pulled low on the ninth pulse.

    I think this is what you are referring to.  A master NACK during the read back byte stops the read back.  In absolute I2C standards probably not but for this part it's ok since you can only access one register at a time and the subaddress register does not auto-increment so doing another byte read will just return the same byte you just read.  A stop essentially kills the transaction anyways.  This is an older device

  • Is there any application Note for the ADV7181C?

    I'm finding difficult to find out which registers to program...

    thanks

  • The design support files can be found at

    https://ez.analog.com/docs/DOC-1621

    It contains a set of scripts to configure the device for operation.