Hi,
I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen.
camera -> 7612 --> 7511 --> screen
When adv7612 output 4:4:4 8bit ycrcb,i can see correct image on the screen,
But when i configure it to 4:2:2,the color is incorrect.
i change two registers:
1)ADV7612: 0x98 03 OP_FORMAT_SEL[7:0]
2)ADV7511: 0x72 15
if there are any other registers i should configure?
thanks,
heven
adv7612 7511
[edited by: heaven at 7:54 AM (GMT 0) on 23 Jan 2019]