Post Go back to editing

CVBS to HDMI conversion

Hi
   Do you have any simple solution which can convert CVBS in to HDMI?

--

  Sebastian V P

Parents
  • FormerMember
    0 FormerMember
on Jan 15, 2019 8:45 AM

The ADV7850 or ADV7842/7511 can convert CVBS to HDMI.  The ADV7850 is a single chip solution but might be over kill for what you are trying to do.

  • Thanks GuenterL.

       You are right, for CVBS alone it is an overkill. We are trying to utilize the other features also.

    May I know the part status? Is it recommended for new designs?

    We are trying to use the VGA conversion also with 3 more additional HDMI mux

    So total inputs will be 1x VGA + 1x CVBS + 3x HDMI

    Does this require DDR Chip in the above application?  

  • FormerMember
    0 FormerMember on Jan 29, 2019 8:37 AM in reply to SebastianVP

    Both ADV7850 and ADV7842 are recommended for new designs.  Check out https://ez.analog.com/video/w/documents/721/read-first-design-support-files-overview

    Only the ADV7850 can handle 3 HDMI inputs.

    The ADV7850 requires DDR while the ADV7842 does not require DDR if you drop 3D comb and TBC features.

    I'd suggest purchasing a EVAL-ADV7850EBZ board for evaluation.

    Note you will have to be an HDCP and HDMI adopter to purchase the 7850 eval board.

  • Reply
    • FormerMember
      0 FormerMember
    on Jan 29, 2019 8:37 AM in reply to SebastianVP

    Both ADV7850 and ADV7842 are recommended for new designs.  Check out https://ez.analog.com/video/w/documents/721/read-first-design-support-files-overview

    Only the ADV7850 can handle 3 HDMI inputs.

    The ADV7850 requires DDR while the ADV7842 does not require DDR if you drop 3D comb and TBC features.

    I'd suggest purchasing a EVAL-ADV7850EBZ board for evaluation.

    Note you will have to be an HDCP and HDMI adopter to purchase the 7850 eval board.

    Children on Mar 14, 2019 11:05 AM in reply to PoornimaSubramani

    The ADV7850 requires DDR if the SDP module is used and in this application CVBS is present so DDR is required.  If if was a ADV7844/7511 solution then external DDR can be dropped if 3D Comb and TCB features are dropped.  Note ADV7844 has 4 HDMI inputs where the ADV7842 has only 2.

    The ADV7850 should be able to handle 4k30.  See private, off-line email. 

    The best bet is to get a ADV7850 reference board and try all the different formats you are interested in.  I personally have not tried 4K30 on the ADV7850 but the spec's say it should work.