Post Go back to editing

Configuration the adv7280m interruption enabled function,but it didn't generate interruption

Hi :

  Configuration the adv7280m interruption enabled function,but it didn't generate  interruption When CVBS signal is detected or lost .

  0x40 0x0E 0x20 

  0x40 0x40 0xD2

  0x40 0x44 0x02

Parents
  • Hi,

    Please refer below Interrupt sequence to configure ADV7182/ADV728x,When the ADV7182/ADV728x locked to a video source or looses video lock.
    Note :
    1) Enter the Interrupt/VDP Map Map by setting register 0x0E bit [6:5] to 01 (binary)
    2) Program the interrupt to drive low when active and to stay low until cleared: In register 0x40 write 0xD1
    3) Unmask (i.e. activate) the lock interrupt: Set register 0x44 bit[0] to 1.
    4) Unmask (i.e. activate) the unlock interrupt: Set register 0x44 bit[1] to 1.
    5) Clear the interrupt. set register 0x43 bits [1:0] to 1.
    6) Exit the Interrupt/VDP Map: set register 0x0E bit [6:5] to 00 (binary).

     

    Thanks,

    Poornima

Reply
  • Hi,

    Please refer below Interrupt sequence to configure ADV7182/ADV728x,When the ADV7182/ADV728x locked to a video source or looses video lock.
    Note :
    1) Enter the Interrupt/VDP Map Map by setting register 0x0E bit [6:5] to 01 (binary)
    2) Program the interrupt to drive low when active and to stay low until cleared: In register 0x40 write 0xD1
    3) Unmask (i.e. activate) the lock interrupt: Set register 0x44 bit[0] to 1.
    4) Unmask (i.e. activate) the unlock interrupt: Set register 0x44 bit[1] to 1.
    5) Clear the interrupt. set register 0x43 bits [1:0] to 1.
    6) Exit the Interrupt/VDP Map: set register 0x0E bit [6:5] to 00 (binary).

     

    Thanks,

    Poornima

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.