I'm having trouble getting the ad9389b to work with all monitors. There are several monitors that I've tried that work fine, but others will either display a shifted video (possibly with artifacts) or no video at all. Below is the i2c registers. It's configured for 720p60. I need this figured out quickly since we're planning to ship this system to a customer.
0 1 2 3 4 5 6 7 8 9 a b c d e f | 0123456789abcdef | |
00: 02 00 18 00 01 22 0a 00 00 00 07 0e 04 10 01 13 | ?.?.?"?...?????? | |
10: 25 37 20 00 02 20 00 03 06 62 04 a8 00 00 1c 84 | %7 .? .??b??..?? | |
20: 1c bf 04 a8 1e 70 02 1e 00 00 04 a8 08 12 1b ac | ?????p??..?????? | |
30: 00 00 00 00 00 41 19 0a 00 2d 00 c0 04 04 10 00 | .....A??.-.????. | |
40: e0 10 60 76 78 80 98 80 00 00 ff ff 00 00 ff ff | ??`vx???........ | |
50: 20 03 00 00 00 00 00 00 00 00 00 00 00 00 00 00 | ?.............. | |
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 | ................ | |
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 | ................ | |
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 | ................ | |
90: 00 00 00 00 c4 c0 20 00 97 02 00 18 38 61 12 70 | ....?? .??.?8a?p | |
a0: 00 00 87 87 08 04 00 00 00 00 00 40 00 00 40 16 | ..????.....@..@? | |
b0: 67 4b 17 02 5a 93 90 4b 20 00 70 ff 00 00 00 00 | gK??Z??K .p..... | |
c0: 00 00 00 00 00 10 16 00 43 03 00 01 02 44 00 70 | .....??.C?.??D.p | |
d0: 70 70 70 70 70 70 70 70 70 70 70 70 70 70 70 70 | pppppppppppppppp | |
e0: 70 70 70 70 70 70 70 70 70 70 70 70 70 70 70 70 | pppppppppppppppp | |
f0: 70 70 70 70 70 70 70 70 70 70 7d aa 1c 00 b0 00 | pppppppppp}??.?. |