Post Go back to editing

[PAL] ADV7393

Thread Summary

The user is trying to configure the ADV7393 to generate a PAL square pixel output from a 16-bit RGB (565) input at 640x480 resolution and 29.5 MHz clock. The final answer confirms that the ADV7393 supports SD non-interlaced mode but cannot convert 288P (SD non-interlaced) to PAL interlaced output. The user needs to provide the correct 768x576 resolution and 25 fps frame rate, with the pixel clock at 14.75 MHz, and ensure proper HSYNC/VSYNC timings as per CEA861B formats 8 & 9.
AI Generated Content

Hi all,

                first of all, thanks for the help you will give us.

Scenario:

- ADV7393 PAL encoder is attached to the output of the LVDS controller of my board. The LVDS output is RGB 16(565) with resolution of 640x480. I would like to generate the output of ADV7393 as PAL signal with SD definition in square pixel mode.

The input clock of ADV7393 is 29.5MHz. My setup of registers is the one reported in table 97 of the datasheet :

Subaddress   Setting                                     Description
0x17               0x02        Software Reset
0x00               0x1C       All DACs enabled. PLL enabled (16×).
0x01               0x00       SD input mode.
0x80               0x11       PAL standard. SSAF luma filter enabled. 1.3 MHz chroma filter enabled.
0x82               0xD3      Pixel data valid. CVBS/Y-C (S-Video) out. SSAF PrPb filter enabled. Active video edge control enabled. Square pixel mode enabled.
0x87               0x80      RGB input enabled.
0x88               0x10      16-bit RGB input enabled.
0x8A               0x0C     Timing Mode 2 (slave). HSYNC/VSYNC synchronization.

Subcarrier frequency register values for CVBS and/or S-Video (Y-C) output in PAL square pixel mode (29.5 MHz input clock).
0x8C 0x0C
0x8D 0x8C
0x8E 0x79
0x8F 0x26

But nothing is snown on my display (PAL) attached to DAC1 of the ADV7393.

- Question:

    - do the LVDS output signal (input of the ADV7393 encoder) have some "constraint" in timing (e.g. HSYNC, VSYNC timing) that will allow the ADV7393 to generate the PAL output ?

    - are my setting correct or I miss something ?

Best Regards,

                A.Biasci.

Parents
  • Hi,

    Have you checked the scripts from Design support files https://ez.analog.com/video/w/documents/801/adv739x-design-support-files

    Please, also try to enable the internal test pattern - register 0x84 bit 6 and check whether the same behavior or not.

    Thanks,

    Poornima

  • Hi Poornima

               we tried to look at your link but we didn't find anything can help us.


    I will try to explain more in details our configuration:
        - we would like to have as output of ADV7393 a PAL (square pixel) signal in CVBS.
        - input data are attached to an LCD controller in 16bit RGB(565).

    We applied table 93 of ADV7393 user-manual (ADV7390/ADV7391/ADV7392/ADV7393 revJ)
    as ADV7393 settings but it didn't show anything on the attached screen to DAC1
    of ADV7393.

    We are not sure about the format of the input signal to provide to ADV7393
    in order to have the PAL output. The CLKIN of ADV7393 is at 29.5MHz and the pixel clock is the same. We are
    able to drive the HSYNC/VSYNC signal of the LCD controller.


    Question:
        - what are the inputs timing and resolution that the LCD controller should
        provide to the ADV7393 in order to see a PAL signal on output ?
            (e.g. HSYNC/VSYNC timing, valid resolution of LCD controller to provide
             to ADV7393, ...).

        - the sentence in datasheet:

                In 16-Bit 4:4:4 RGB Mode, the pixel data is updated at half the rate of the clock, that is, at a rate of 13.5 MHz (see Figure 6)

           is valid also for SD square pixel mode ?



    Best Regards,
            A.Biasci.

  • Hi,

    16-Bit 4:4:4 RGB mode is Only external syncs can be used though in this mode, not embedded syncs.
    The clock would obviously be half normal at 13.5Mhz as well.
    Note: Embedded EAV/SAV timing codes are not supported with SD RGB mode.Also, master timing mode is not supported for SD RGB input mode, therefore,external synchronization must be used.


    Square Pixel Mode can be enabled by register 0x82[4]. Note that for CVBS and S-Video  (Y-C) outputs,
    the SD subcarrier frequency registers must be updated to reflect  the input clock frequency used in SD square pixel mode.Also note that the SD  input standard auto detection feature must be disabled in SD square pixel mode  (this is disabled by default after reset)
    Apply the clock and enable internal color bars. If you have programmed correctly you should get proper color bars and color sub carrier output.After that configure the input to math the format you are applying.

    Thanks,

    Poornima

  • Hi Poornima,

                              thanks for your reply. We are modifying our prototype to achive the half-rate pixel clock.

    Some more question:

    • are there any constraint on HSYNC/VSYNC timing in SD square pixel mode?
      • e.g. HSYNC should be Xns
      • e.g. VSYNC shoul be Yms
    • can I provide, as input, an RGB 4:4:4 with 640x480 as active resolution, coming directly from LCD controller or the input signal must have the resolution of SD square pixel standard?

    Thanks again for your help.

    Best Regards,

                    A.Biasci.

  • Hi,

    For NTSC operation, an input clock of 24.5454 MHz is required. The active resolution is 640 × 480.

    For PAL operation, an input clock of 29.5 MHz is required. The active resolution is 768×576.

    The output from this part seems to be programmable, which should enable you to output the exact timing expected at the encoder.And also ADV7393 can only provide external syncs based on EAV/SAV time codes that it receives. It can't generate timing

    Thanks,

    Poornima

  • Hi Poornima,

                       thanks again for your help. Let me summarize for PAL square pixel:

    • 29.5MHz is the clock to provide to ADV7393
    • 14.75MHz is the pixel rate to provide to ADV7393
    • 16 bit RGB 4:4:4 is the output of my LCD controller (input of ADV7393)
    • the resolution to provide as input to ADV7393 (output of my LCD controller) is 768×576
    • frame rate is 25 fps
    • HSYNC/VSYNC timings are reported in the table above

    So ADV7393 does not performs any scaling/adjusting of the input signal. It "only" performs a sampling of digital data to provide, as output, a signal compliant with PAL square pixel (supposing I configured the chip correctly).

    Are this summary correct? I will provide to you a feedback once we have the solution in place.

    Best Regards,

                 A.Biasci.

  • Hi,

     Yes,ADV7393 cannot do any scaling,It can only support the formats indicated in Table 1 of the datasheet.

    Thanks,

    Poornima

Reply Children
  • Hi Poornima,

                        thanks for your help. Unfortunately, we still have problem to configure the chip. Question:

    • the input provided to ADV7393 to produce an output compliant to PAL-square pixel mode, must be interlacced?

    Best Regards,

                        A.Biasci.

  • Hi,

     Yes, ADV7390/ADV7391/ADV7392/ADV7393 support an SD non-interlaced mode. All input configurations, output configurations,and features available in NTSC and PAL modes are available in SD non-interlaced mode.

    Thanks,

    Poornima

  • Dear Poormina,

                         I couldn't find this kind of configuration in the ADV7393 datasheet Rev J. Could you help me?

    The Table 63 on page 92 of the datasheet, for SD-mode, always reports as Input Format an interlaced mode but not progressive.

    Progressive Input Format(s) are reported only in Table 98 on page 99 for Enhanced Definition.

    Regards,

          A.Biasci.

  • Hi,

     Please refer Page52 in datasheet for more details about SD non-interlaced mode.

     

    Thanks,

    Poornima

  • Dear Poornima,

                  thanks again for your help. Could you confirm our setup in order to generate a PAL square-pixel output:

    • CLKIN is 29.5MHz
    • Pixel Clock is 14.75 MHz
    • Input Format is 16 RGB565 --> 756x288p
    • Output of ADV7393 is CVBS

    We are trying to calculate the timings of LCD controller to generate the correct signal at 756x288p to provide as input to ADV7393.

    Questions:

    • there are a reference timing that HSYNC/VSYNC signals must have?
    • there is a constraint about the time between HSYNC and the first valid pixel of the frame?
    • there is a constraint about the time between VSYNC and the start of the new frame?

    Datasheet does not report any timing about our configuration (SD noninterlaced mode), so any help will be very appretiated.

    Best Regards,

    A.Biasci.

  • Hi,

     I beleive,ADV7393 does support 288p digital in and will output this as 288P analogue video. It cannot convert 288P (SD non-interlaced) to PAL interlaced output.

    The timing we are expecting is described in CEA861B formats 8 & 9. We do not publish output video timing formats in datasheets.

    Thanks,

    Poornima

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.