Post Go back to editing

AD8194

Hi everyone,

I've a PCB with an AD8194 and AD9880. The AD8194 mux is connected to a DVI and HDMI connector.

I've a trouble with the AD8194. The AD9880 doesn't detect signal with some DVI sources like personal computers.

If I remove the AD8194 and I do a bypass with some wires, the AD9880 detects the video source. Please, could anybody help me?

Thank you

Best regards

Jose

Parents
  • Hi Dave,

    I have replaced the AD8194 and the result is the same.

    In fact I've probed DVI with several tft monitors and the result is the same in all of them. I can't see image on the screen. I only see image if I remove the AD8194

    I think you're right, the sources of DVI are damaged

    I've measured the source of DVI in other PC with problems and the results are:

    CLK+ it's ok (The AVcc and Vswing are right)

    CLK- it's ok

    TMDS 0+ it's ok

    TMDS 0- it's ok

    TMDS 1+ it's ok

    TMDS 1- it's ok

    TMDS 2+ it's ok

    TMDS 2- it's wrong. I have a countinuous 3.3v more less

    I attach some images of the measures before and after of AD8194

    I don't understand why the AD9880 works fine if I remove the AD8194? It's a bit strange

    Thank you

    Regards

    Jose

Reply
  • Hi Dave,

    I have replaced the AD8194 and the result is the same.

    In fact I've probed DVI with several tft monitors and the result is the same in all of them. I can't see image on the screen. I only see image if I remove the AD8194

    I think you're right, the sources of DVI are damaged

    I've measured the source of DVI in other PC with problems and the results are:

    CLK+ it's ok (The AVcc and Vswing are right)

    CLK- it's ok

    TMDS 0+ it's ok

    TMDS 0- it's ok

    TMDS 1+ it's ok

    TMDS 1- it's ok

    TMDS 2+ it's ok

    TMDS 2- it's wrong. I have a countinuous 3.3v more less

    I attach some images of the measures before and after of AD8194

    I don't understand why the AD9880 works fine if I remove the AD8194? It's a bit strange

    Thank you

    Regards

    Jose

Children
No Data