Post Go back to editing

AD8194

Hi everyone,

I've a PCB with an AD8194 and AD9880. The AD8194 mux is connected to a DVI and HDMI connector.

I've a trouble with the AD8194. The AD9880 doesn't detect signal with some DVI sources like personal computers.

If I remove the AD8194 and I do a bypass with some wires, the AD9880 detects the video source. Please, could anybody help me?

Thank you

Best regards

Jose

Parents
  • Hi Jose,

    The dc common-mode voltage of the CLK + and - lanes should be the same and should be AVcc - 250mV  The minimum logic low level for DVI should be AVcc - 600mV.  It would appear as though the DVI sources are non-compliant or damaged.   What are the CLK signal levels when connected directly from DVI source to AD9880?   It is possible that the AD8194 might have been damaged by and ESD event.  Have you tried replacing the AD8194?

    I do not think your issue is related to the AD8194 equalizer.

    Best Regards,

    Dave

Reply
  • Hi Jose,

    The dc common-mode voltage of the CLK + and - lanes should be the same and should be AVcc - 250mV  The minimum logic low level for DVI should be AVcc - 600mV.  It would appear as though the DVI sources are non-compliant or damaged.   What are the CLK signal levels when connected directly from DVI source to AD9880?   It is possible that the AD8194 might have been damaged by and ESD event.  Have you tried replacing the AD8194?

    I do not think your issue is related to the AD8194 equalizer.

    Best Regards,

    Dave

Children
No Data