Using ADV7184 SCART Overlay with ADV7341, isolated pixels are faint

Hi,

I am using the ADV7184 back to back with an ADV7341, to add an RGB overlay over CVBS. I find that when pixels are isolated, with no adjacent pixels in the same line, they are considerably dimmer. This means that vertical lines appear dark and text is of inconsistent brightness.

I thought this may be the the encoder attempting to filter noise, so I experimented with various DNR gain levels and filters but I did not notice a difference.

Here is an example, note how the vertical and diagonal lines in the image are much darker than the horizontal lines.

Vertical and horizontal lines

Is there some way to avoid or mitigate this effect, and have all overlay pixels of the same brightness?

Thanks!

Parents Reply Children
  • 0
    •  Analog Employees 
    on Nov 13, 2018 2:01 PM in reply to peter_k

    Hi,

    For overlay applications, text can be more readable if the contrast of the video directly behind the text is reduced.
    Due to the higher bandwidth, the signal transition of the luma component is usually much sharper than that of the chroma component.
    The color edge is not sharp and can be blurred, in the worst case, over several pixels.  
    Chroma transient improvements are needed primarily for signals that have severe chroma bandwidth limitations.
    For these types of signals, it is strongly recommended to enable the CTI block via CTI_EN.
    For more information Please refer Chroma transient improvement and contrast reduction section in the datasheet.

    Thanks,

    Poornima

  • Thanks Poornima, I will experiment with the CTI block and see if that improves things. 
    Reducing the contrast behind the video text does make the text more readable, in fact I have it enabled in the image above. 

  • 0
    •  Analog Employees 
    on Nov 15, 2018 7:37 AM in reply to peter_k

    Hi,

    Please crosscheck the encoder and decoder clocks.To Selecting the clock frequency one over the other may be desirable in systems in which board cross talk between different components leads to undesirable interference between video signals. It is recommended to use a crystal of frequency 28.63636 MHz to clock the ADV7184. Is this issue reproducing from encoder or decoder side?

     

    Thanks,

    Poornima

  • Hi,

    Here is what I have found so far.

    Enabling/disabling CTI in the decoder makes no appreciable difference.

    Enabling/disabling DNR and changing the gain in the encoder makes no appreciable difference.

    Enabling FB Edge Enhancement makes the effect slightly worse (although barely noticeable), and the effect becomes worse as edge enhancement level is increased. I would have expected the opposite.

    Slowing down the pixel clock for the RGB overlay does improve things because the overlay pixels become wider and chroma has more time to stabilise, but the result is decreased horizontal resolution and rectangular pixels.

    I am clocking the decoder with a 28.63636 crystal and I'm not encountering crosstalk.

    I can't tell at this stage whether the effect is occurring in the encoder or decoder because I don't have a way to capture the digitized video stream from the decoder and display it. However the effect does not go away if I change the output of the ADV7341 from CVBS to YPbPr, which suggests that it is occurring within the decoder/encoder circuit rather than limitation in chroma bandwidth when decoded by the video monitor.

    It is also definitely a chroma effect, I don't notice a problem with white or grey overlay text.

    Do you have any other suggestions?

  • 0
    •  Analog Employees 
    on Nov 19, 2018 1:57 PM in reply to peter_k

    Hi,

    Please try to adjust the chroma filter register to set different bandwidth in both encoder and decoder part.
    Refer ADV734x datasheet, here chroma filters listed in table 43 and the ADV7340/ADV7341 contain an SSAF filter that is specifically designed for the color difference component outputs, Pr and Pb. This filter has a cutoff frequency of ~2.7MHz and a gain of –40 dB at 3.8 MHz (see Figure 62). This filter can be controlled with Subaddress 0x82, Bit 0.Please refer chroma filter section in the ADV7184 datasheet .   

    Note : Chroma Shaping Filters (CSH):The shaping filter block (CSH) can be programmed to perform a variety of low pass responses. It can be used to reduce selectively the bandwidth of the chroma signal for scaling or compression.      

    Thanks,

    Poornima