KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD723
Production
The AD723 is a low cost RGB-to-NTSC/PAL encoder that converts analog red, green, and blue color component signals into their corresponding luminance and...
Datasheet
AD723 on Analog.com
Hello,
I have questions about AD723.
The start point of color burst from AD723 seems to move on AD723 Eval Board (AD723EB rev.B).
Could you see attached file "Color_burst_AD723_rev01.xlsx" for more detail?
Thank you!
Best regards.
Tamu
Hello Tamu,
Process variations would produce a fixed delay in the path, so the phase ambiguity would still be the same. Power supply level would also produce a fixed delay, as long as it stayed constant. There may be an insignificantly small variation in delay as the supply is varied, but this can be ignored since it would be much, much less than 90 degrees at 3.579545 MHz (about 70 ns).
Frequency errors in the external 4FSC source will result in corresponding frequency errors in the colorburst and chroma subcarrier frequency. If the colorburst is used at the receiver to recover the chroma subcarrier reference, there will be no subcarrier-related errors in the chroma demodulation.
Best regards.
--Jonathan
Hello Tamu,
Process variations would produce a fixed delay in the path, so the phase ambiguity would still be the same. Power supply level would also produce a fixed delay, as long as it stayed constant. There may be an insignificantly small variation in delay as the supply is varied, but this can be ignored since it would be much, much less than 90 degrees at 3.579545 MHz (about 70 ns).
Frequency errors in the external 4FSC source will result in corresponding frequency errors in the colorburst and chroma subcarrier frequency. If the colorburst is used at the receiver to recover the chroma subcarrier reference, there will be no subcarrier-related errors in the chroma demodulation.
Best regards.
--Jonathan