KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD723
Production
The AD723 is a low cost RGB-to-NTSC/PAL encoder that converts analog red, green, and blue color component signals into their corresponding luminance and...
Datasheet
AD723 on Analog.com
Hello,
I have questions about AD723.
The start point of color burst from AD723 seems to move on AD723 Eval Board (AD723EB rev.B).
Could you see attached file "Color_burst_AD723_rev01.xlsx" for more detail?
Thank you!
Best regards.
Tamu
Hi Tamu,
I don't have the schematic that shows exactly how the colorburst is gated. The block diagram you attached is very high-level and essentially shows pictorially what is described by the phrase in my earlier reply that you quoted, so I'm not sure what you are asking. The same description is given in the data sheet.
The fact remains that the Hsync and 4FSC signals are asynchronous. The counter that is clocked by 4FSC is enabled when the falling edge of the Hsync pulse reaches its nominal midpoint, but the phase of the 4FSC clock is indeterminate at that point in time because it is not synchronous with the Hsync signal. The 4FSC phase could, therefore, be anything between 0 and 2pi when the counter is enabled. This is where the ambiguity comes from, which amounts to 90 degrees at the colorburst frequency. The phase of the colorburst will change by the same amount each time it is inserted because the Hsync signal and 4FSC signal are cycle-slipping relative to each other at a constant rate. (If you put the two asynchronous signals on a scope and triggered on one, the other would be seen to slip past the one that the scope is triggered on.) This is the main source of the phase ambiguity. Propagation delays will introduce a fixed time shift, but the variations, or deltas, will be due to the cycle-slipping. Any variations with temperature will be small enough to ignore.
Best regards.
--Jonathan
Hi Tamu,
I don't have the schematic that shows exactly how the colorburst is gated. The block diagram you attached is very high-level and essentially shows pictorially what is described by the phrase in my earlier reply that you quoted, so I'm not sure what you are asking. The same description is given in the data sheet.
The fact remains that the Hsync and 4FSC signals are asynchronous. The counter that is clocked by 4FSC is enabled when the falling edge of the Hsync pulse reaches its nominal midpoint, but the phase of the 4FSC clock is indeterminate at that point in time because it is not synchronous with the Hsync signal. The 4FSC phase could, therefore, be anything between 0 and 2pi when the counter is enabled. This is where the ambiguity comes from, which amounts to 90 degrees at the colorburst frequency. The phase of the colorburst will change by the same amount each time it is inserted because the Hsync signal and 4FSC signal are cycle-slipping relative to each other at a constant rate. (If you put the two asynchronous signals on a scope and triggered on one, the other would be seen to slip past the one that the scope is triggered on.) This is the main source of the phase ambiguity. Propagation delays will introduce a fixed time shift, but the variations, or deltas, will be due to the cycle-slipping. Any variations with temperature will be small enough to ignore.
Best regards.
--Jonathan