Post Go back to editing

ADV7612 16BIT SDR

i want the adv7612 output 16bit YCbCr with vsync ,hsync and de.

I sellect 16BIT SDR ITU-BT-656 Mode 0 with set the value  98,03, 80

the regs value setting :

98 ,00, 02,

98,01, 06,

98,02, F5,
98, 03, 80,
98, 04, 62,
98, 05, 29,
98, 06, A6,
98, 0B, 44,
98, 0C, 42,
98,14, 7F,
98,15, 80,
98,19, 83,
98,33, 40,

44,BA, 01,

64,40,81

68 9B 03 ; ADI recommended setting

68 00 08 ; Set HDMI Input Port A (BG_MEAS_PORT_SEL = 001b)

68 02 03 ; Enable Ports A & B in background mode

68 83 FC ; Enable clock terminators for port A & B

68 6F 0C ; ADI recommended setting

68 85 1F ; ADI recommended setting

68 87 70 ; ADI recommended setting

68 8D 04 ; LFG Port A

68 8E 1E ; HFG Port A

68 1A 8A ; unmute audio

68 57 DA ; ADI recommended setting

68 58 01 ; ADI recommended setting

68 75 10 ; DDC drive strength

68 90 04 ; LFG Port B

68 91 1E ; HFG Port B

when i change the Resolution to 1920*1080, there display,but a litter time ,it disapper,

is there any problem with regs setting .