Are there any differences of register settings we should set between ADV7511 and ADV7511W?

Hello,

I have questions about the register settings of ADV7511 and ADV7511W.

Question:

Are there any differences of  register settings we should set between ADV7511 and ADV7511W?

I think that "ADV7611 evaluation board software release 1.56.0 ALPHA" includes source code for ADV7511 (not for ADV7511W).
https://sdk.analog.com/dw/sdks.aspx?file=ADVSW15
Can we use these source code for ADV7511W without changing any register settings?

Background:
My customer has been developing HDMI repeater system using ADV7611 and ADV7511W.
They use your "ADV7611 evaluation board software release 1.56.0 ALPHA" module.
So we'd like to know whether he can use it for ADV7511W without changing any register settings or not.

Thank you!
Best regards.
Tamu

Parents
  • 0
    •  Analog Employees 
    on Oct 4, 2018 12:30 PM

    The ADV7511 and ADV7511W are the same die.  The basic differences are:

    • ADV7511 does deep color up to 225MHz, ADV7511W is limited to 165MHz, no deep color
    • Packages are different.  Smaller input data bus.
    • ADV7511W is targeted for automotive applications,  it is screened for a wider operating temperature range and reliability.

    If the customer does not need deep color than the ADV7511W will work.

Reply
  • 0
    •  Analog Employees 
    on Oct 4, 2018 12:30 PM

    The ADV7511 and ADV7511W are the same die.  The basic differences are:

    • ADV7511 does deep color up to 225MHz, ADV7511W is limited to 165MHz, no deep color
    • Packages are different.  Smaller input data bus.
    • ADV7511W is targeted for automotive applications,  it is screened for a wider operating temperature range and reliability.

    If the customer does not need deep color than the ADV7511W will work.

Children