Post Go back to editing

ADV7189b abd ADV212 Interfacing Problem

Hi all!

I have made a Video Encoder board following the exact schematic as of P160 Evaluation Kit with the host-controller being a DSP rather than an FPGA. I have been able to configure ADV212 successfully and read back the application id (0xFF82). I also configured ADV7189B according to the recommended settings in the datasheet. I read back all the registers from ADV7189B and matched with what I had actually written. All the registers match the programmed value except for 3 registers at addresses 0xD0,0xD5 and 0xD7. The value read back from these registers does not match the ones I have written. The recommended settings in datasheet were for CVBS input at AIN5 but in my case it is at AIN1 so I changed the value at 0x00 register accordingly. After connecting the camera, I read the status register of ADV7189B and find that its lock bit is asserted and the format detected is also correct (PAL). However, ADV212 SCOMM[3:0] pins are constantly held at a value of 0x7 (after configuration) which indicates that it is waiting for the video. I checked the HS,VS,Field and signals of ADV7189B and they appear to be generated correctly. I have tried both input format, HVF as well as embedded EAV/SAV, in ADV212 encode parameters but no difference observed.So, I have the following queries:

1) What can be the reason that registers 0xD0,0xD5 and 0xD7 does not return the same value as written to them?

2) Is there any register in ADV7189B to control inclusion or exclusion of EAV/SAV information in pixel data?

3) How can it be verified that the pixel data output by adv7189b is correct?

4) What configuration missing in adv212 or adv7189b can cause this type of problem?

5) If both ICs are supposed to be working fine what other issue can it be?noise or ringing on pixel data bus?

6) What other observations can be made to drill down the problem?

Thanks in advance!

Regards,

Shaji

  • Hi Shaji,

    What VFORMAT are you using for PAL? '1' or '9'? 

    Dave

  • I am using PAL 4:2:2 i.e VFORMAT set to '1'

  • Hi Shaji,

    It looks like your connection are ok from your schematics and if you are using '1' then it's not the problem I thought and it's likely the ADV7189B output is not PAL for some reason. As to your specific questions above:

    1) They could be write-only registers... many of the "recommended settings" registers are.

    2) NEWAVMODE (should be a 1), BT656-4 (1 for NTSC and not relevant for PAL), SD_DUP_AV (0).  I don't think you can turn off AV Codes.

    3-5) You can't really verify the pixel data but verifying syncs is what's important.  I would check that the syncs are in the right place for PAL as the ADV212 expects. It's the inactive edge of VSYNC that kicks off the timing so the active edge should be on line 23 after the inactive edge (or V bit). If it's seeing that then it should make it past state "7" at least. Can you put a scope and get H, F, and V around a blanking period?

    Noise on syncs could cause a problem but it would have to be pretty bad-- same with noise on data and it would only matter on the time codes.

    Dave

  • I have attached the waveforms as output by ADV7189B and seen on logic analyzer. It appears that field and VS signals are synced with each other but HS signal is not synced with them. Secondly the number of HS active low pulses each time is different (114,90 etc.). If you need to know the timings please let me know I will email the measured timings also.

    Please suggest probable cause of the problem and its solution.

  • Hi Shaji,

    The H Sync is clearly very wrong-- it should be going all the time but it looks like it's stuck high most of the time.  That would definitely cause the problem.

    Have you checked how the ADV7189B is programmed on the P160? The software is on our FTP site and it should be in there.  I really don't see how any misprogramming could cause it to fail like that but that should be your focus I think.

    Dave

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.