Post Go back to editing

About ADI Recommended Write of ADV7182 in ADV7128CUST-VER2.6.txt

Dear support team,

Could you tell me briefs of each ADI Recommended Write in ADV7128CUST-VER2.6.txt,please?

42 5A 90 ; ADI Recommended Writes

42 60 B0 ; ADI Recommended Writes

42 0E 80 ; ADI Recommended Writes

42 B6 08 ; ADI Recommended Writes

42 C0 A0 ; ADI Recommended Writes

42 D9 44 ; ADI Recommended Writes

42 0E 00 ; ADI Recommended Writes

I want to know the adverse effect for system ,when this setting is not used

Best regards,

Takepiro

  • Hello Takepiro,

    ADV7128 is an obsolete product.  Do you mean it or ADV7182?

    In either case, those writes are generally determined at characterization and we don't disclose the details except to say you must write them.


    Dave

  • Dear Dave-san,

    Thank you for your supports.

    Sorry.It is ADV7182.

    "ADI recommended Write" infomation are in only script file.

    So, our product doesn't have "ADI recommended write",now.

    I understood that we should add them to our product.

    But,stage of development is almost final.

    So,we should explain tha mean of addtional register writeing to add them for internal and end customer.

    Could you tell me the outline of these registers,please?

    Best regards,

    Takepiro

  • Dear Dave-san,

    Thank you for your supports.

    I think that there is not recomended settings document of ADV7182.They are in only script file.

    Could you tell me only which part in the device even influences it by "ADI recommened register" setting,please?

    ( ex: 42 5A 90 ; ADC optimization.)

    If these information doesn't exist, the register settings cannot be added.

    Best regards,

    Takepiro.

  • Hello Takepiro,

    There should be a recommended settings document that has them also.  If those writes are not included, I would not expect the part to work reliably (unless those values are default anyway).

    Those registers are generally internal settings that let us handle process variation which is why they are determined during characterization. The settings that show up as "ADI Recommeded Settings" are the values that work reliably across voltage and temperature. They really should be called "ADI Required settings"

    Dave

  • Hi Takepiro-San,

    Coincidentally I have just updated the ADV7182 script to version 3.0 today. This contains more comments than version 2.6 as well as free-run scritps. I am currently trying to update the ADV7182 design support files page with this new script.

    Also note that the ADV7182 datasheet contains descriptions of all customer registers. See I2C Register Maps section of ADV7182 Rev.A Datasheet. http://www.analog.com/static/imported-files/data_sheets/ADV7182.pdf

    regards,

    Robert Hinchy

    Applications Engineer,

    Analog Devices

  • Dear Robert-san,

    Thank you for your supports and Updating the script.

    I checked it.

    But, about "ADI recommended Write" register,  there is no additional information in this script.

    I want to know the outline of register of "ADI recommended Write".

    Could you tell me about them,please?

    Best regards,

    Takepiro.

  • Hi Takepiro-San,

    These writes are for internal engineering reasons. We  generally do not share these with customers. Therefore I will not be posting this information up on the Engineering Zone forum.

    However I have been communicating with the Analog Devices' Japanese FAE team to try and deal with your concerns. I believe that you are also in contact with them.

    I think that it would be better if you communicated directly with the Japanese FAE team rather than via this forum. This should allow us to deal with your questions and prevent confusion in communications. 

    Thanks and Regards,

    Robert

  • Dear Robert-san,

    Thank you for your suppports.

    I will contact to Japanease FAE team.

    Thank you and best regards,

    Takepiro

  • Hello Takepiro-San,

    I have updated the ADV7182 script files. The new scripts can be found at the ADV7182 Design Support files website.Note that all the writes given in the scripts are required for the correct operation of the ADV7182.

    I have also created an ADV7182 recommended settings document. This goes into more details about these writes. This document is also available on the design support files website.

    Link to ADV7182 Design Support Files:

    http://ez.analog.com/docs/DOC-2633

  • Dear Rob-san,

    Thank you very much for your supports.

    I already got the document.

    Thank you very much and best regards,

    Takepiro