Article What is the highest output waveform frequency of the PWM ports on the MAX7315?

The 32kHz internal PWM oscillator has a timeslot that is divided into 15 master intensity timeslots. Theoretically the fastest output you can achieve is 32kHz / 15 which is roughly equal to about 2kHz using some combination (say 8/16) of the individual timeslots per master slot. The oscilloscope shots on page 5 and Figure 11 can help to visualize the output based on different individual and master register settings. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.