MAX

  • Created
Was this helpful?
  • How do I implement a constant power output?

    As an example, it can be implemented with MAX17503 + MAX4211 + MAX4163 + MAX16904: The MAX17503 can output 12V, with a maximum current of 2.5A. This serves as the input power source. Depending on system…
  • Is there a MAX4570EVKit?

    Answer: No. The MAX4550EVKIT was used for evaluating the MAX4570 (required replacing the MAX4550 with the MAX4570), but the evkit is no longer available, and there are no plans to offer this in the future…
  • Is there a replacement or upgrade for MAX13362?

    The MAX20091 is an upgrade for MAX13362. This IC can monitor 35 channels, whereas MAX13362 can monitor 24 channels. MAX20091 is available in a 48-pin TQFN package. MAX13362 is avilable in a 40-pin…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.