For the ADV7842 this FAQ answers the following questions,
1. - List all the supported input 3D formats and resolutions.
2. - Does it support 3D to 2D conversion.
3. - All the output format it supports…
Question The CEC and Hot Plug pins on the HDMI interfaces are not specified
as 5V tolerant in the data sheet, but they may experience 5V signal
levels in my design.
Can they withstand 5V signals…
Attached and linked below are several files supporting the development of systems using the ADV7842 .
File
Content
ADV7842 Product Page
Link to ADV7842 Product Web Page
ADV7842…
Question Could you provide the schematic of the eval board for ADV7842? Answer On the EngineerZone in "ADV7842 Design Support Files" at
http://ez.analog.com/docs/DOC-1712
You could download "ADV7842…
This FAQ applies to EVAL-ADV7842-7511 and EVAL-ADV7842-7511P. All support files in their latest versions will be attached below.
Below are the support files for these evaluation board. We recommend that…
We provide the attached scripts in order to assist customers with validating their hardware (boards) based on the ADV7842.
For customer product software, we recommend that customers license the source…
44 is the CP Map in the below script
To get start_sav:
WRITE:
44 A1 01 ;
44 BB 00;
44 BC A0;
READ:
44 FC
44 FD
To get start_eav:
WRITE:
44 A1 01 ;
44 BB 00;
44 BC B0;
READ:…
The attached document gives a general CP core gain overview as well as precise details on how gain is calculated, why we need to gain our signal and how to optimize for the best setting on your system…
Q: Please provide some guidance for required register write sequencing in ADV7850. This is not all clear in the Recommended Settings document.
A: I2C sequencing in our scripts associated with the evaluation…
1. Does ADV7842 say Audio sample packet detected in case incoming signal is PCM or IEC61937 as explained in page 219 (UG-214.pdf). If so, how we can further detect between PCM and AC3.
[ANS] The audio…