Hi
Attached is script for evaluation boards:
EVAL-ADV7611EB1Z,
EVAL-ADV7611EB2Z,
EVAL-ADV7612EB1Z,
EVAL-ADV7612EB2Z
It gets 576i (2x) and outputs as an 656 stream 8-bit to encoder. Encoder outputs it as CVBS.
Same script will work for 480i after changing encoder settings to 480i.
Scripts for 656 8/10/12-bit require not only setting appropriate OP_FORMAT_SEL, but also doubling the clock (In red)
Same applies to ADV7619.
Best regards,
vito
This FAQ was generated from the following discussion: 8-bit 656 script for ADV7611EB1Z, ADV7611EB2Z, ADV7612EB1Z, ADV7612EB2Z, ADV7619