Hi
Attached is script for evaluation boards:
EVAL-ADV7611EB1Z,
EVAL-ADV7611EB2Z,
EVAL-ADV7612EB1Z,
EVAL-ADV7612EB2Z
It gets 576i (2x) and outputs as an 656 stream 8-bit to encoder. Encoder…
Hue adjustment is done on YCrCb data stream;
It can be done in CP-core by:
Enabling video adjustmnets (VID_ADJ_EN, CP-core, 0x3E[7] in ADV7611/2/9)
Setting hue to desired value (CP_HUE, CP-core…
Attached and linked are several files supporting the development of systems using the ADV7611 .
If you download and use these documents, we recommend that you subscribe to notifications for this post…
ADV7611, ADV7612 scripts for 576i to HDMI out by vito
Hi
Attached script that takes in 576i (625i) HDMI in and gives output through encoder.
This can be run in XRC. To be used with following boards…
We have provided the scripts for a number of our HDMI products in order to assist customers with validating their hardware (boards).
Please note that for customer product software, we recommend that…
We provide the attached scripts in order to assist customers with validating their hardware (boards) based on the ADV7611.
For customer product software, we recommend that customers license the source…
Original Question: CVDD's bypass capacitor of ADV7611. by Tamu
Hi,
I have some questions about your recommendation of CVDD's bypass capacitor of ADV7611. Please refer attached file "Questions CVDD…
The ADV7842 can indicate if the input is encrypted or not.
This can be read back in the HDMI Map
Register 0x05[6] - Content encrypted.
Register 0x04 [4] – HDCP Key Error ( this will be set if for…
Few things often forgotten during reviews of ADV7611, ADV7612., ADV7619 and other schematics;
First - It is suggested to follow recommendation from Design Support Files pages:
For 7612: https://ez…
Using the LIMIT_MCLK_OUTPUT_FREQUENCY.XLS file in the link below, it is possible to limit the minimum and maximum MCLK output frequencies from the HDMI receivers. For example, select the desired maximum…