Programming Zynq on Adalm PLuto using Vivado

Hello everyone,

I am currently working on a project where I should implement an FFT ip core on the zynq of my Adalm Pluto. I used an Adalm UARTJTAG card that I connected to the Adalm Pluto, then I plugged a digilent  programming cable (JTAG HS3) onto the Adalm JTAGUART card, and connected the JTAG HS3 to the PC through the mini USB cable.

The problem is that the JTAG cable is not detected by the Xilinx SDK, so I have the following questions :

Are my connections right ? are these the right tools to be used ? if yes, is there any hardware drivers that I should install (and in which directory should I put them) ? On the xilinx SDK, should I "Program FPGA" or "Program Flash" ?

I would be very grateful if you could answer my questions because I searched everywhere but couldn't find any solution to my problem.

PS: - I am using Vivado 2016.4 

       - The zynq on my adalm pluto is Zynq Z7010

       - OS : Windows 7

Thank you in advance.

Kind Regards.