PRECISION COUNTER TIME MODULE FOR ADLAM2000 SCOPY

Hi

I need a high precision, high resolution (thirty two bit)  timer/counter for measuring real-time-clock crystal oscillators, using a GPS Disciplined 10 MHz external signal as the reference on one input  and gating this over  a couple of minutes on a second input. I was going to build one, but then came across the ADALM2000 and Scopy.  Sadly there doesn't seem to be a counter/timer function provided.

Physics labs often use such counters for photon and geiger counting so a counter/timer function sort of fits with the project objectives.

I would think the hardware would have no problem doing this. 

Are there any plans for this?

What would be required to program the ADLAM2000 to enable this functionality. i.e.

- Development environment

- Debugging hardware etc.

Rob Garnett

Toongabbie