AnsweredAssumed Answered

Sepic ?

Question asked by zanzibar on Nov 4, 2011
Latest reply on Nov 4, 2011 by LucaV

Hi,

 

I need to design a power supply with :

*  Input  voltage = 11,5V

*  Output  voltage = 10 V  or 12V

* output current = 1A

Output voltage needs to go from 10V to 12V very fast, this can be selected with a transistor on the feedback pin for example.

 

Which solution do you recommend ?

Outcomes