AnsweredAssumed Answered

ZC706+AD9467

Question asked by ccruztorre on Oct 16, 2017
Latest reply on Oct 18, 2017 by ccruztorre

Sometimes when I program ZC706 FPGA in SDK and Run software, nothing appears in UART console and XMD console shows command running and the process never stop. If I debug it doesn´t work. I turn off the target and after repeating the same procedure, the system starts to work

It doesn´t seem to be the ADC board or the UART connection (It is checked  successfully). It seems that the FPGA is not well programmed when system_top.bit is uploaded

Have you got any suggestion? or have anybody experienced the same issue?

Thanks

Outcomes