AnsweredAssumed Answered

JESD link is not working on DAQ2 and ZCU102 hardware setup

Question asked by James12345 on Oct 12, 2017
Latest reply on Nov 8, 2017 by James12345

 Hi guys,

 

I am trying to avoid raising this problem in an old question thread.

 

We loaded up the latest dev branch (yesterday) of both HLD and no-OS. Using vivado 2017.2.1 and SDK 2017.2, building HDL bitstream and no-OS app was not a problem.  Then, we had a few go of no-OS on zcu102. Now, configuring ADC/DAC seems to work now. (well done!). Below is output of uart. It suggests that jesd link between daq2 and zcu102 is not working.

 

Can we have a bit more information about this problem?

Cheers,

James

 

jesd_status jesd_status: not in data phase (10)!
jesd_status jesd_status: out of sync (3)!
adc_setup adc core initialized (1000 MHz).
dac_setup dac core initialized (1000 MHz).
ad9144_status : CGS NOT received (6)!.
ad9144_status : ILAS NOT received (0)!.
ad9144_status : framer OUT OF SYNC (0)!.
ad9144_status : check-sum MISMATCH (0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x0, 0x0 0xA1A0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x0, 0x1 0xB1B0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x0, 0x2 0xA1A0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x0, 0x3 0xB1B0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x1, 0x0 0xC1C0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x1, 0x1 0xD1D0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x1, 0x2 0xC1C0, 0x0)!.
ad9144_short_pattern_test : short-pattern-test mismatch (0x1, 0x3 0xD1D0, 0x0)!.
ad9144_datapath_prbs_test : PRBS OUT OF SYNC (1)!.
ad9144_datapath_prbs_test : PRBS I channel ERRORS (FF)!.
ad9144_datapath_prbs_test : PRBS Q channel ERRORS (FF)!.
ad9144_datapath_prbs_test : PRBS OUT OF SYNC (5)!.
ad9144_datapath_prbs_test : PRBS I channel ERRORS (FF)!.
ad9144_datapath_prbs_test : PRBS Q channel ERRORS (FF)!.
daq2: transmit data from memory
daq2: RX capture done.

Outcomes