AnsweredAssumed Answered

H.264 software module linked with uClinux tool chain

Question asked by BlairFredericks on Nov 3, 2011
Latest reply on Nov 26, 2011 by BlairFredericks

Hi,

 

There is a H.264 software module that available with Visaul DSP++

 

This like says it is not possible in a Linux enviroment.

http://docs.blackfin.uclinux.org/doku.php?id=visualdsp:port_program_to_linux

None of this information will help you link VDSP++ object files with gcc object files, or allow you to run VDSP++ objects in a Linux environment.

 

However can this precompile lib archive "libh264enc_BF561_48.dlb" be linked  using uClinux tool chain so it can be ran as a bare metal applcation  along with ICC on core B, while running uClinux on core A?

 

Under the heading Misc, it seems to suggest it is possible.

http://docs.blackfin.uclinux.org/doku.php?id=visualdsp:port_linking

 

If not, is there any way somone could get a hold of the source so they could port it.

Would seem to be ashame have this great component and not be able to use it in this context.

 

Thanks,

 

-Blair

Outcomes