AnsweredAssumed Answered

ADuCRF101 1kHz interrupt

Question asked by kli on Nov 2, 2011
Latest reply on Nov 7, 2011 by kli

Hello, sorry for asking a very basic question. Can someone give me a piece of sample code in C language of generating 1 kHz interrupt in ADuCRF101? The part is operating off 16MHz system clock frequency. I need to trigger an off-chip event at 1 kHz. I guess I might use the GP timer freely runs counting, when overflow, it should trigger an interrupt to trigger the external event... Unfortunately I'm not familiar with embedded C coding. So it'll be great if someone can provide a sample code. thanks in advance.

Outcomes