AnsweredAssumed Answered

CN0349 Application Questions

Question asked by mike.baker Employee on Oct 5, 2017
Latest reply on Oct 5, 2017 by Brandon

I'm interested in using the CN0349 CFTL as the basis for a product and have a few questions.

  1. Are the outputs temperature compensated conductivity readings or just the analog values?
  2. Can this be used for water?
  3. Is the calibration implemented in the GUI the same as outlined in the AD5934 data sheet?
  4. Is there any reason the calibration routine and set-up implemented in the GUI can't be implemented in the BF527?
  5. Is the source code used for the GUI available for embedding in the BF527?
  6. Is there a spare SPI port on the BF527 for use connecting to our system?

 

Thanks for the support...

Outcomes