AnsweredAssumed Answered

AD9517 reference input differential DC coupling

Question asked by thomaslap on Oct 4, 2017
Latest reply on Oct 4, 2017 by pkern

I am developing an application which uses the AD9517 PLL. The reference frequency should accommodate a range of 0.5 to 100Mhz. As input interfacing standard, we can still choose, as long as it is differential (LVDS, CML, LVPECL[2.5V or 3.3V])

 

Since the lower boundary is below 1Mhz, DC coupling is suggested in the datasheet. The datasheet states that for DC coupling the voltages need to be matched to the self-biasing voltages of the REFIN inputs. This is the part that is confusing. Which standards can the REFIN differential accommodate with DC coupling, how should these be matched and terminated?

Outcomes