AnsweredAssumed Answered

About ADM1186  On/Off sequence

Question asked by Yuya on Oct 2, 2017
Latest reply on Oct 10, 2017 by Yuya

 Hi,

I would like to use ADM1186.

So, I have some questions.

 

About On sequence

#1  Is it OK if VIN4 is 0.6V or more at the timing of ENABLE OUT4 active?

 

About Off Sequence

#2  Does the internal status and PWRGD signal operate asynchronously?

 

#3  If VIN1 to VIN4 are 0.6V or more, will PWRGD become active?

 

#4  During off sequence operation, do not control DELAY only, are they also matching with the recognition that is   

    performing power monitoring?

 

Since it can be from one, please give me an answer earlier.

 

Best Regards,

Yuya

Outcomes