AnsweredAssumed Answered

Failed to connect to processor with SC584 and CCES

Question asked by macci77 on Sep 26, 2017
Latest reply on Oct 3, 2017 by Kader.M

When I connect ICE1000 to SC584 EZBoard and try to debug an example code with CCES, it complains as follows:

 

[TpsdkServer] Failed to connect to processor.

Error: 0x80048015
Error Description: Initialization: Open device driver failed

 

 

ICE1000 's LED lights with green color.

I tried changing/updating the driver etc. but nothing helped

--------------------------------------

Solution to this:

 

To overcome this problem we did as follows:

I noticed that McAfee had been downloaded without my knowing of it and saw there was some contradiction in the parameters.

 I first uninstalled McAfee Web Advisor. That didn't fix the problem. Next, I used regedit to search for all occurrences of "mfesapsn". There were several, including, 

HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Enum\Root\LEGACY_MFESAPSN
HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Class\{78A1C341-4539-11D3-B88D-00C04FAD5171}


It is the GUID in the latter that conflicts with the Analog Devices CrossCore Tools class, which causes its installation to fail. I'm not sure whether deleting the LEGACY_MFESAPSN registry entry(s) was necessary, but I did delete them.

I also had to manually change permissions on several of the registry keys and some subkeys before I was successful at deleting them.

Outcomes