AnsweredAssumed Answered

I'm using ADCUM360 evaluation board (old version) with 8 pin header for debugging Can I use a standard segger J-LINK and where can I find the connection diagram ?

Question asked by alwinvantol on Sep 25, 2017
Latest reply on Sep 25, 2017 by barryzhang

evaluation board with J-LINK debug interface

 

I Blew up the J-LINK module, This module is not for sale by mouser, farnell and so on.

 

Where can I buy this module, or can I use a standard Segger J-LINK module ? 

Where can I find the connection diagram to connect the pin header on the Segger J-LINK module with 8 pin header on the evaluation board, because it looks like if the 8 pin header on the evaluation board is not a standard J-TAG interface.

 

With the J-LINK module provided by Analog Device it is possible to debug and setup a serial (COM) connection at the same time. Is this also possible with the J-LINK module from Segger ?

Outcomes