AnsweredAssumed Answered

I would like to ask: the problem of AD9851 on the use of two DDS signal synchronization...

Question asked by xi_yan on Sep 23, 2017
Latest reply on Sep 26, 2017 by mcee

1. Using AD9851, respectively, for two single-chip, can not achieve two output signals with the same frequency 、amplitude、same phase?
2. If the two microcontrollers are far apart and not on the same board can achieve two output synchronization?
3. Through the programming of the microcontroller, set the same parameters, can achieve the function of synchronization?
4. Is it appropriate for other suitable DDS chips?

Outcomes