AnsweredAssumed Answered

How to enable HW timestamping in PTP

Question asked by ThierryNolf on Sep 22, 2017
Latest reply on Sep 25, 2017 by Gregchen

I was able to compile Linux with PTP for the EZ-kit SC589.

 

Although the datasheet describes that hardware timestamping in the MAC is supported, I was not able to configure the linuxPTP (ptp4l) to use hardware timestamping, on none of the two EMAC's.

 

Also the timestamping in the Phy doesn't work.

 

The result of the <ptp4l -m -f ptp4cfg.cfg > command is :

interface 'eth0' does not support requested timestamping mode

 

The same goes for eth1 when changed in the config file.

 

The linux compilation is the one as can be downloaded in the cces-linux-add-in version 1.2.0.

 

Enclosed the config file

 

Br,

 

Thierry Nolf

Attachments

Outcomes