AnsweredAssumed Answered

I have a half Bridge CN0196-EB1Z and few question: is the circuit 12V isolated to VDD? If yes, which circuit and voltage is their possible? I need circut up to 350A and voltage up to 500V by 5 to 30kHz. What can I do or what must I do get-at-able? Fritz

Question asked by Ignatia on Sep 22, 2017
Latest reply on Sep 26, 2017 by glai

Hi,

I have a Half-Bridge CV0196-EB1Z and few question: Is the circuit 12V isolated to VDD? If yes,which circuit and voltage is their in VDD possible? I Need circuit up to 350A and voltage up to 500V by 5 to 30kHz at the output. What can I do, or what must I do get at able?

Fritz

Outcomes