AnsweredAssumed Answered

About  AD9670 Evaluation Boad

Question asked by Yuya on Sep 21, 2017
Latest reply on Sep 21, 2017 by AshrafS

Hi,

I would like to use AD9670.

So, I have some questions.

 

#1  What is the purpose of the EXTERNAL SYNC pin of the capture board (HSC_ADC_EVALZC)?

 

#2  Is data output correct as it is output from 16 data output pins of FPGA?

 

#3  When sending the signal converted from the ADC evaluation board to HSC_ADC_EVALZ, is there information such

   as the definition of the time from the start of data acquisition by the ADC to the output of the data on the HSC board,

      error, accuracy, etc?

 

Best Regards,

Yuya

Outcomes