AnsweredAssumed Answered

Is there a bass sub harmonic generator block? Like the opposite end of "superbass")

Question asked by PloppyThirds on Sep 20, 2017
Latest reply on Oct 14, 2017 by KJBob

My goal is low frequency output enhanced as low as 8Hz (or lower, as a rotary woofer is in discussion.) Common audio does not include tones this low - usually bottoming out around 32Hz - so to reinforce sound with infrasound these tones must be synthesized from the existing subwoofer range in the audio stream. As I understand from other posts the superbass block only generates tones above the cutoff I want to generate tones below it.

Outcomes