AnsweredAssumed Answered

How to use ADV7613 to drive two identical LVDS display panels

Question asked by wilson_wan on Sep 20, 2017
Latest reply on Sep 22, 2017 by edo

Hi,

  The ADV7613 is an HDMI input device, with dual transmitter LVDS output, so I try to use ADV7613 to drive two identical LVDS display panels, now the ADV7613 can drive only one panel, I try to write 0x04 to Address  OLDI Map, 0x4E, but the lvds pll lost lock.

   "In the dual LVDS transmitter mode, the output formatter blocks splits a single video data stream into two separate streams, the even pixel stream is output on LVDS Transmitter 1, and the odd pixel stream is output on LVDS Transmitter 2."

   so what could be the problem? should I double the pixels, just like pixel repetition?

  thanks.

Outcomes