AnsweredAssumed Answered

AD7626 CNV signal duty cycle

Question asked by lopez.zoni on Sep 19, 2017
Latest reply on Sep 20, 2017 by Gnib

Hi,

 

In the AD7626 datasheet says:

 

Table 3: CNV High Time has a maximum value of 40ns.

Self Clocked Mode Section: Conversions are initiated by a CNV± pulse. The CNV± pulse must be returned low (tCNVH maximum) for valid operation. 

 

If I were to have an sampling rate of 10MHz than I have a period of 100ns. I should not use a %50 duty cycle since that will make CNV signal high for 50ns.  So the duty cycle needs to be maximum 40%.

 

When I examine the Evaluation Module for AD7626, the AD9513 clock OUT 0 is configured to be 50% duty cycle.

 

This confused me. Can you please explain what I miss here?

 

Regards

Outcomes