AnsweredAssumed Answered

Freq range of AD-PZSDR2400TDD-EB

Question asked by Kalkikrishna on Sep 18, 2017
Latest reply on Sep 27, 2017 by Neil.wilson

In the LNA-PA module AD-PZSDR2400TDD-EB, the LNA's operating frequency range is given as 1.7GHz to 2.2GHz, but how this module can be working with 2.4GHz. Whether this board can be interfaced with FMCOMMS2 board, if so whether through the FMC connector or through the P202 header. What is the purpose of P202, only test point, Why this header is given without any ground connections. Why the "technical details/data sheet/user guide/manual" for AD-PZSDR2400TDD-EB is not available as single pdf/pdfs. We had to go through many web pages to get information still we feel it is not complete. Thank you

Outcomes