AnsweredAssumed Answered

Question about the relationship between DEV_CLK_IN and IQrate?

Question asked by @MTU on Sep 14, 2017
Latest reply on Sep 14, 2017 by @MTU

Modified AD9528_Evaluation_Board and input REF CLK = 98.304 MHz.
(C407 / C409 implementation, R414 / C408 removal)

 

I set AD9371 as below.
 DEV_CLK_IN = 98.304MHz
 IQrate     = 49.152MHz

 

The following error occurred.

 

  Mykonos pllStatus = 0x1L
  MCS Status =  0xbL
  System.Exception: Error Programming ARM: ERROR:452, ARM system problem has been detected.


     at AdiCmdServerClient.Mykonos.loadArm(String fileName)
     at Microsoft.Scripting.Interpreter.ActionCallInstruction`2.Run(InterpretedFrame frame)
     at Microsoft.Scripting.Interpreter.Interpreter.Run(InterpretedFrame frame)
     at Microsoft.Scripting.Interpreter.LightLambda.Run4[T0,T1,T2,T3,TRet](T0 arg0, T1 arg1, T2 arg2, T3 arg3)
     at System.Dynamic.UpdateDelegates.UpdateAndExecute3[T0,T1,T2,TRet](CallSite site, T0 arg0, T1 arg1, T2 arg2)
     at Microsoft.Scripting.Interpreter.DynamicInstruction`4.Run(InterpretedFrame frame)
     at Microsoft.Scripting.Interpreter.Interpreter.Run(InterpretedFrame frame)
     at Microsoft.Scripting.Interpreter.LightLambda.Run2[T0,T1,TRet](T0 arg0, T1 arg1)
     at IronPython.Compiler.PythonScriptCode.RunWorker(CodeContext ctx)
     at IronPython.Compiler.PythonScriptCode.Run(Scope scope)
     at IronPython.Compiler.RuntimeScriptCode.InvokeTarget(Scope scope)
     at IronPython.Compiler.RuntimeScriptCode.Run(Scope scope)
     at Microsoft.Scripting.Hosting.CompiledCode.Execute(ScriptScope scope)
     at IronPythonWindow.ScriptHost.Execute(String expression)

Do you know the cause?

 

I do not know the setting of the value of Mykonos.init_clocks and the value of Mykonos.init_rxProfiles.
Could you tell me how to set it when IQrate = 49.152 MHz?

 

Link.Mykonos.init_clocks(98304, 7864320,Link.Mykonos.VCODIV.VCODIV_2, 4)
Link.Mykonos.init_rxProfiles(1, 2, 2, 5, 1, 1, 49152, 10000000, 10000)
Link.Mykonos.init_txProfiles(1, Mykonos.DACDIV.DACDIV_2p5, 2, 2, 1, 1, 49152, 10000000, 100000000, 100000, 100000)

 

I attach python script.
AD9528_98.304M.py : AD9528 setting
init_98M_int.py   : AD9371 setting

Outcomes