AnsweredAssumed Answered

HMC1110 current for VD_MULT unclear in datasheet

Question asked by BDeutschmann on Sep 13, 2017
Latest reply on Sep 27, 2017 by BDeutschmann

In the HMC1110 datasheet on page 1 there is the current for VD_MULT given in the table as 80mA.

But below it says: '[2] Adjust VG_X2, VG_X3 between -2 to 0V to achieve 1 - 2 mA on VD_MULT.'

 

So I'm wondering which is the right current for the device 1-2mA or 80mA.

 

Here is the link to the mentioned datasheet:

http://www.analog.com/media/en/technical-documentation/data-sheets/HMC1110.pdf 

Outcomes