AnsweredAssumed Answered

Hi, Is the ADA4895-1 suitable for making an active low pass filter(like an integrator), I want the gain factor more than 20, and I'm not sure whether this amp is suitable for this application since there is no such recommendation in the datasheet.

Question asked by yang_xu on Sep 11, 2017
Latest reply on Sep 19, 2017 by JinoL

Hi, Is the ADA4895-1 suitable for making an active low pass filter(like an integrator), I want the gain factor more than 20, and I'm not sure whether this amp is suitable for this application since there is no such recommendation in the datasheet. It works well as an non-inverting pre-amp, but once I add some capacitor the signal becomes quite noisy. 

Outcomes