AnsweredAssumed Answered

Phase and Amplitude measurement by using AD9364

Question asked by Inter on Sep 9, 2017
Latest reply on Sep 11, 2017 by Vinod

Hi,

 

I need to measure the amplitude and phase of a FMCW signal (1.5GHz~5GHz). Can I use AD9364 to measure the amplitude and phase of input signal? Otherwise, can I do FFT to the output of ADC then get the amplitude and phase? If no, is there another transceiver IC can do it, like AD9375.

 

I'm still waiting for my 9364. Thank you very much.

Outcomes