AnsweredAssumed Answered

ADIS164x5 tilt accuracy

Question asked by rcm on Sep 7, 2017
Latest reply on Sep 12, 2017 by NevadaMark

Hello,

 

I have a similar request as [ https://ez.analog.com/docs/DOC-15776 ].

 

My basic requirements for accelerometer are:

 

Tilt range: ±30°
Tilt accuracy: ±0.1° [I'll use a precision 3 axis turntable (±0.01°) to recalibrate my system after final assembly].
Operating temperature: 0°C to 50°C.

 

My question is: Do ADIS16445 (Preferred) or ADIS16485 comply to my needs?

 

Thanks in advance.

Outcomes