AnsweredAssumed Answered

SYNC multiple HMC7044 in simple Divider Mode

Question asked by hoo on Sep 7, 2017
Latest reply on Sep 21, 2017 by kpeker

Q1:

multiple slave HMC7044s in simple Clock Divider Mode with 3GHz clock input from CLKIN1,both PLLs are power down and only output Divider is used.is it possible to SYNC those slave HMC7044s ?

Q2:

the output delay can still be used in this Clock Divider Mode?

Q3:

SYNC and SYSREF share the path,a SYNC pulse should be sent first to align all the DCLKs,then the path is given to SYSREF,what's the configuration procedure,the datasheet give no much details.

 

Thanks

Outcomes