AnsweredAssumed Answered

Could you please consider  and share additional knowledge about the following aspects:  1)     How to сorrect this?  2)     what registers to consider for correct work?  3)     How to properly configure the AGC mode? 

Question asked by SAnton on Sep 5, 2017
Latest reply on Sep 8, 2017 by Vinod

The AD 9361 operates in half-duplex mode. Transmission time and reception time of 10 ms, pause between transmission and reception of 1 ms. Modulation mode BPSK, speed 6 Mbps, mode of operation AGC "Fast attack". At low signal levels (of the order of -80 dBm), normal operation is ensured (reception without data loss). When the level of the input signal is increased (to -45 dBm), the losses of the first packets are observed. 

Outcomes