AnsweredAssumed Answered

ADuC7023 GPIO setting for JTAG pins

Question asked by jhshin on Sep 4, 2017
Latest reply on Sep 18, 2017 by mark.ramos

Currently, my customer has a problem that P0.1/0.2/0.3 sometimes do not work properly as GPIOs.

 

When the customer uses P0.1/0.2/0.3 as GPIOs, the setting sequence is as follows.

1) Set BM=1, 0x80014=0xFFFFFFFF on reset

2) User code reconfigure the pins as the GPIO mode via the GPxCON/GPxDAT register

2) If it needs user code download, customer uses I2C download via set BM=0 on reset

 

Q1- Is there a problem with the above settings ?

Q2- How should the customer set up ADuC7023 to use P0.1/0.2/0.3 as GPIOs reliably without error?

 

Thanks.

Outcomes